This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8304: Dead time adjustment questions

Part Number: DRV8304


I’m looking at DV8304H and calculating losses for different MOSFET power stages.

The datasheet states that the dead time is not a fixed value, but has a typical value of 120ns for the HW version of the DRV8304.

Is it correctly understood that DRV8304 adjusts the dead time automatically, dependent on the switching time of the MOSFET? If so, why is it possible to adjust the dead time on the SPI device?

 I’m looking at MOSFETs that have 30ns-60ns in switch on time and 10ns to 30ns in switch off time - My concern is that if the typical dead time is 120ns, it will result in significant power losses due to the freewheeling diode.

  • Carlos,

    Please check sections 7.3.1.4.2 for explanation. Basically there is standard "fixed" base dead-time inserted and then the device automatically adjusts the needed dead-time up from there using the technique listed in 7.3.1.4.2.

    Regards,

    -Adam