This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8873: Capacitor between CPH and CPL

Part Number: DRV8873

Hello,

Our customer use the DRV8873H.

The customer worry about poor supply of capacitor parts. Especially, the parts that its size as larger than 0603 are rare.

They use the DRV8873H with 24V VM. So, they are looking for over 35V tolerant parts.

The capacitor of 35V tolerant and 47nF, there is only large size parts.

Do you have any idea?

Best Regards,

Naoki Aoyama