This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8873: DRV8873: Is DVDD generated in SLEEP?

Part Number: DRV8873

Hi,

Asi in topic: Is 5V on DVDD pin generated in SLEEP mode?

It seems that it is not but I want to be sure.

BTW Would be good to have this information in datasheet.

Regards,

Pawel