This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8886AT: How to reduce hold(stop) current of stepper motor

Part Number: DRV8886AT


Hi,

Does TI have a DRV with the function to reduce the hold current of a stepper motor?

Our customers use the ONSEMI : STK672-632A-E. This hybrid product has two excitation current modes, which can reduce the current while the motor is stopped.
According to the DRV8886AT data sheet, is the description in the section “7.3.5 Controlling RREF With an MCU DAC” a function that meets the customer's request?
Customers will use both bipolar and unipolar stepper motors.
Best regards,
Hiroshi
  • Hi Horishi-san,

    The TRQ pin can be used to change the hold current to 75% or 50% of the Ifs value. Please see Table 5 for details.

    If the hold current desired is different than 75% or 50%, the current flowing through the RREF pin can be adjusted as described in section 7.3.5.

    Another method is to use two resistors in parallel at RREF with a switch on one resistor.
    The hold current uses one RREF resistor, and operating current uses both RREF resistors in parallel.
  • Rick-san

    I'm sorry that I failed to make sure.

    Thank you for your advice.
    Best regards
    Hiroshi