How do I:
1. set up eeprom for motor
a. we have set up the parameters in the chip EEPROM and have the motor running using the pot on the EV board
b. can I somehow capture the settings and sequences that go from the PC gui app to the EV board?
2 run the motor - can I just write to one or two of the registers or do I have to follow a flow chart?
3. stop/brake the motor - again, can I just write to one or two of the registers or do I have to follow a flow chart?
4. reverse the motor?
5. what is important in monitoring the motor
6. can i hold the motor without moving perhaps by energizing just one phase - typically (100 ms or so)
7. change speed while running?