#define USER_ZEROSPEEDLIMIT (0.5 / USER_IQ_FULL_SCALE_FREQ_Hz)
The actual test found that: USER_ZEROSPEEDLIMIT value is too large (greater than 2.0) is more likely to jitter, too small (less than 0.5), motor startup is weak, instantaneous overcurrent, routine default value of 0.5, has not yet found a suitable value, which value of this parameter is better to start with load?