This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8313: continuous phase current for DRV8313

Part Number: DRV8313

Hello,

What is the continuous phase current for DRV8313 in RMS?

What is maximum allowable pwm frequency for DRV8313?

Regards,

Mohammad.

  • Mohammad,

    The datasheet lists this information.

    The outputs are rated for 2.5A RMS each. The overcurrent trip point is at 3-5A.

    The Recommended Operating Conditions table lists the PWM frequency upper max at 250kHz.

    Regards.

    -Adam