Dear Sirs,
My customer system is under burn-in testing and found there is abnormal FAULT pin signal occurred.(LED turn on).
The fail rate is around 30% with total 1400pcs.
While the LED turn on, the motor will stop, or the pulse # of moving step is wrong.
Customer used 4pcs per system and from the highest failure rate to low is IC10>IC11>IC9>IC8
The PCB is FR4 and the thickness is 1.6mm, copper thickness 1oz.(TI EVM is 2oz)
Attached is the schematics and please help to check if there is anything need to be modify.
Thanks.