Part Number: BOOSTXL-DRV8323RS
Other Parts Discussed in Thread: LAUNCHXL-F28069M, BOOSTXL-DRV8301, MOTORWARE, DRV8323, LAUNCHXL-F280049C, , BOOSTXL-DRV8320RS
I would like to control two PMSM motors simultaneously.The motor specs are-
- Power - 400 W
- Vdc = 50 V
- halls sensors inbuit
The best way I could see if the use of LAUNCHXL-F28069M + DRV8323RS (2). However, when i started to look into the lab documents, it says that the dual motor can only be used with BOOSTXL-DRV8301 or BoostXL-DRV8305.
Is this a case because the DRV8323RS is a new booster pack and the pdf is not updated?
If not, what could I use instead?instaspin_labs.pdf, Thanks in advance