Part Number: DRV8833
Hi all
Would you mind if we ask DRV8833?
There is the description "fPWM Current control PWM frequency = 50kHz" on the datasheet.
Does it mean that this frequency is for current control PMW light?
It is not relation to input PWM, right?
For example, we assume as follows;
Input PWM=5Hz -> Output freqency = 5Hz.
Kind regards,
Hirotaka Matsumoto