Other Parts Discussed in Thread: DRV8353
Hello TI team,
I need to clarify some technical topics, that will influence the decision of choosing DRV8353S or DRV8353RS variant of the chip. Mr. Klenk Benjamin recomended to ask directly the quiestion on this forum.
1) Is the internal buck regulator completely separated internally, from the main circuit die ? (in two separated dies) I need this info for the DFMEA.
2) VM supply current is stated into the datasheet for 48V (Table 7.5 Electrical Characteristics) and no PWM input. I will need this current for 17V, considering the CP different operating point. If possible, a graph of VM input current variation for the whole input voltage range, will be very useful (17V to 48V considering 25mA load on HS and 25mA on LS). Second case, 17V-48V but only 12mA HS-CP load and VGLS load.
3) DVDD regulator can supply an external load of 10mA, and probably is the supply for the internal digital core of DRV835x-xx. Is this Idvdd already considered in VM total current specified for 48V (typ 8.5mA) ?
Thank You !