Hello,
I am going to use DRV8889 in one of my upcoming project.
From Datasheet of DRV8889, I found that there is Control Input STEP, DIR used to control the Direction and Step of the Motor. There is SPI Interface is also available.
My Question is that : Can we use the SPI to manage the Function of STEP and DIR? If Yes then what should be the electrical condition of STEP and DIR Pins(Pull Down or Pull up)?
Regards,
Alpesh