Other Parts Discussed in Thread: DRV8847
I have an existing product using a motor driver from another vendor, but need to switch, and am considering the DRV8884 (or similar). The main application is for small, bipolar stepper motors (~5V models), but there is a desire to drive 12V unipolar stepper motors also. I have seen designs where this is done without changing the way the motor is wired (just changing the drive current and step rate). That is, the common center tap on the unipolar motors is left open. I have tested this, and it works, but it seems to me that it cannot be driving it optimally since (1) it is putting 12V across 2 coils in series instead of the intended single coil, and (2) the coil on the other side of the center tap is also being driven at the same time, although it is effectively driven with reverse polarity (+6V on 1 coil and -6V on the other). I'm a little baffled at how this could work at all, but the real question is whether there is a better way to do it. Specifically, shouldn't the center taps (from both sets of coils) be connected to the +12V supply? A coil that is driven to 12V by the drv8884 chip is then effectively OFF, while the GND side coil has the full 12V across it, as intended.
Thanks,
Greg