Part Number: DRV8308
Hi,
I have such a problem. The sygnol on the leg FAULTn log.0 is constantly except when the RESET is high.
The engine is running. It is possible to reset errors in the 0x2A register, it will be state 0, but this does not change the signal on the FAULT pin, it will be low 0.
The RESET signal is given when ENABLE low. What kind of error and how to diagnose it. The engine is operating normally.
Appreciate for the answer. Vyacheslav