Other Parts Discussed in Thread: DRV10983
Hi. I need help in choosing a component for a bldc motor controller. I have a project that will use a bldc motor running from 4 v to 14 v maximum current 1A, without a sensor. I want to place the speed controller directly onto the motor board size 22 mm. I want it to be as simple and reliable as possible. Motor speed control should be at the expense of voltage from 4 to 14v from a separate DC power source. I read a lot of information on bldc motor drivers but I have too little experience with this. I chose the DRV10975 componentbut I don’t understand how I can implement engine speed control due to the strength of the constant current.