This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8702-Q1: Can full-bridge driving circuit for a large current BDC motor be configured using two of DRV8702?

Part Number: DRV8702-Q1
Other Parts Discussed in Thread: DRV8702D-Q1

 Hello guys,

 One of my customer is considering using DRV8702(half-bridge gate drive).

 Also they want to drive a large current BDC motor (Idrv is 20A~30A) with full-bridge circuit for CW/CCW turning and breaking.

 They have the follwoing question. Could you please give me your answer?

 Q. Can a full-bridge driving circuit for such large current BDC motor be configured using two of DRV8702?

 Your reply would be much appreciated.

 Best regards,

 Kazuya Nakai.