Hello,
I am newbie at motor drivers,
I want to design BLDC driver via 8332.
I checked the application diagram at the data sheet.
I need help about resistors.
There is a 3.3 ohm resistor at PVDD source
and
There is a 1 ohm resistor between AGND and GND
What are the purpose of these resistors and which package(watt) should i use?
I am going to supply 48V.
Motor RMS 6A
Motor Peak 9A
resistor watt of 3.3 ohm PVDD = V2/R = 48*48/3,3 = 698W???
And one more question:
https://katalog.we-online.de/pbs/datasheet/742792903.pdf
Is this ferrite bead suitable for my design. In the datasheet, it says "10 ohm or higher at 10mhz or below". It looks suitable but I want to be sure.