I'm using a DRV10983EVM to drive a small BLDC 2POLE motor and after loading correct parameters into the driver chip using TI software the motor is running good.
The I tried using MIKROE-2766 and loaded all the same setting and I can't get the motor to work.
The two schematics look exactly the same. I'm getting a U Pole falt. Maybe the driver chip is bad on the MIKROE board.
Has anybody tried this MIKROE board before and had any success.
The DRV10983EVM is about $100 and the MIKROE board is only about $20 and it's mostly just the driver chip on both.