This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8320: RGZ package

Part Number: DRV8320

Hello,

A customer sent screenshots of different variations of RGZ packages (RGZ0048L, RGZ(S-PVQFN-N48), RGZ0048D). His questions below:

1. Is the RGZ package generic? I.e., for part numbers that include "RGZ", does it mean they all use the same "RGZ" package?
2. Drawings have different dates, are these just old versions of RGZ?
3. Are the pad sizes specific to the part number?

Thanks!

  • Elisha,

    The package has evolved throughout the years. The latest drawing is the one you should be using.

    Each part may have a drawing that works best for it so please always use the datasheet for the part you are using.

    Regards,

    -Adam