This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SNBB028N's question

Hi all

Would you mind if we ask SNBB028N?
This is special product for the customer, so is it possible to confirm on E2E?

<Customer's situation>
Vref=3.3V
Isense=3.3Ω
-> Itrip = Vref/(5×Rsense) = 200mA
In case of I=High : 200mA -> OK
In case of I=Low  : 80mA -> NG
If I is low setting, the current is limited 12%. So it might be 24mA originally.
Therefore, to break down this failure into parts, we consider follow;
-To confirm customer's circuit
If you have some advice, could you let us know? 
We atttach the wave form file;
20190618_SNBB028N_Waveform.pdf

And then, we would like to send cusomer's circuit and datasheet using private message on E2E or directly.
My E-mail address : matsumoto-h@macnica.co.jp

Kind regards,

Hirotaka Matsumoto