Other Parts Discussed in Thread: DRV8886, DRV8886AT, DRV8711, DRV8842
Hi Experts,
Can DRV8876 use for stepper motor?
Best Regards,
Fujiwara
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Fujiwara-san,
It is possible to use two DRV8876 to drive a stepper. But there are restrictions.
1) If using internal current regulation, only slow decay is available.
2) If using IPROPI to regulate the current, slow decay and fast decay are available.
a) Fast decay (Hi-Z) may pull too much current out of the coil.
b) Fast decay using reverse or forward may reverse the current.
c) The IPROPI current is not available for all decay modes.
With these restrictions, it is recommended to use a stepper motor driver like the DRV8886 or DRV8886AT with internal current regulation and multiple decay modes available.
What is the VM voltage and current of the motor?
Hi Rick-san,
Thanks for the answer. VM is 26V and current (full-scale) is 3.5A. Do you have any recommended device? DRV8886 cannot handle 3.5A current.
Best Regards,
Fujiwara
Hi Fujiwara-san,
The DRV8711 with external FETs is a good choice.
Also two DRV8842 (one for each coil) will work.
The DRV8711 has a Step/Direction interface and requires fewer control inputs. It also has a SPI interface to configure the device.
Assuming microstepping is desired, the DRV8842 requires additional control signals to set the proper current levels. At a minimum, control of IN1, IN2, and VREF is needed to adjust the direction and level of current.