Other Parts Discussed in Thread: MSP430F5529
Tool/software: Code Composer Studio
Hi,
I am currently using DRV8323RS with MSP430F5529 to run a sensorless BLDC motor.
I am trying to create a standalone program without the use of GUI.
With DRV8323RS, I downloaded the source code for sensored and sensorless for CCS.
I managed to create a program for sensored motor and is able to run the sensored BLDC motor
However, when I tried to replicate the codes for the sensorless BLDC motor, the motor doesn't turn on. I measured the voltage at the high and low gates and noticed that GLA, GLB, GLC is reading some voltage (~ 10Vdc) while GHA, GHB, GHC is reading 0V. I believe that is incorrect.
Is it possible to have a look at my codes? If yes, I can send you my codes in a separate email if necessary.
Please advice.
Appreciate your help.
Thanks,
Thena