This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV120: Looking to limit hold current to 15-20mA.

Part Number: DRV120
Other Parts Discussed in Thread: DRV110

DRV120 has a min hold current of 40mA.  

Is it possible to achieve hold current to 15-20mA, 100mA for peak?

Is there any issue with placing a series R between the solenoid and the out to limit current this way?

 

The other option would be DRV110, which has an external FET, but integrated is preferred.