Other Parts Discussed in Thread: DRV8323
We use DRV8323S IC in our design.On the Power on process,DRV8323S runs with error occasionall :GHA/GHB/GHC run in a wrong waveform when PWM_IN was kept low,as attached. In the sys_attachment.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We use DRV8323S IC in our design.On the Power on process,DRV8323S runs with error occasionall :GHA/GHB/GHC run in a wrong waveform when PWM_IN was kept low,as attached. In the sys_attachment.pdf
Hello,
Please confirm if this behavior occurs before or after the device has been programmed over SPI to change to 1X PWM mode.
Since you have hall signals going into the device and the device powers up in 6X pwm mode, the device might be trying to act on the hall signal inputs.
Regards,
-Adam
Hi Adam :
TKS for help.
It is confirmed that this behavior occurs before device has been programmed over SPI,and It is sure that there is no PWM signal input。
It only occurs about 1/5 on the Vmotor power on process.
Hi Adam :
We have more information after further testing.
Hello,
1. There is no EEPROM or flash. You will need to program is every time.
2. You will need to remove hall power or disconnect the halls with a buffer/mux if you want to avoid this.
3. See above.
Regards,
-Adam