Part Number: DRV8885
Hi Team,
My customer is using DRV8885, for the current regulation, what it means "Full step (2-phase excitation) with 71% current" in the datasheet (page 28)?
Does it mean that, for example, you set 1A threshold and actually it triggers OCP @710mA?
Because the customer did observe this phenomenon. For 1/16 step, 1/2 step and 1/4 step etc., the measured OCP current conforms to equation (5), but for full step, the setup threshold is 400mA, but the measured OCP is approximately 300mA.
thanks a lot.
Yang