This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8305: SPI register set issue

Part Number: DRV8305
Other Parts Discussed in Thread: TMS320F28069M,

Hi TI team,

We are facing issues configuring the DRV8305 chip with a TMS320F28069m processor. Example : I would have 1 ampere on the IDRIVEN_HS, IDRIVEP_HS, IDRIVEN_LS, IDRIVEP_LS but when I have set the IDRIVEN_HS at 1A and I try to set the IDRIVEP_HS the value returned by the DRV8305 is not the one I sent it. 

I have the same behaviour on all the control registers and it is critical for us. Can you help ?

Thanks