Hi,
We would like to work with DRV110 @ peak current of 2.5A, and hold current of 1.5A.
Is this possible? From the datasheet eq.2 and 3 it is unclear what Rsense should be.
If it is possible, can you please recommend Rsense?
We are going to use DAC instead of the Rpeak and Rhold.
DAC voltage is 0-1V.
Do we still need Rpeak and Rhold if using a DAC to limit the current?
if so, what are the values?
Thanks a lot