This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Sensorless BLDC Motor Driver IC

Other Parts Discussed in Thread: DRV8353R, DRV8323

Hi, 

I'm looking for a solution, controlling my Sensorless BLDC Motor
Specs of motor

Power: 150W 

Current rating: 12A

Max. Vol: 50v

operating Voltage: 28.8v

an example of motor willing to control PM Brushless Motor, 


Type -BM70-0.4H
Serial No. 351900009
100watt at 3000RPM
3Ph. 17Volts-200Hz IP-54
duty continuous, Class-F



any lead is highly appreciable

Thanks and Regards
Sonu Verma
R&D