This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Customer is considering to use DRV8837 or DRV8838 to achieve a lower current consumption during suspend mode when the chip is not functional (with no input from pin5/pin6.) They can support two input as PWM or non-PWM input control, may I know if there's a difference of suspend mode consumption between these two chips? Or you have a even better proposal other than these two chip to achieve a lower suspend mode consumption?
Thanks!
Antony
Hi Antony,
A better way to minimize power consumption when entering sleep mode is to set all inputs as a logic low to minimize systems power. This way, the power consumption is lowered by eliminating the current through the internal pulldown resistors.