This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8323: Show Current Fault on Phase A and Phase C

Part Number: DRV8323

As i had design my New DRV8323 board V2 . the previous version work very well. I not change anything but only i  just reduce the size  from 128 X 50 mm  to 50 X 73 mm .As it show  current fault on phase A and C . rest i  also got  ringing on SPI . So i am not able to understand the  previous board work well and just making it compact not it not able to drive motor . In my previous design I use  3 resistance to measure current in all the three phase , Bur now i use  2 resistance in parallel  where one side of resistance connect to three   lower MOSFETs and other part of resistance is connected to Ground.