This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8885: setting M0 and M1 about DRV8885

Part Number: DRV8885
About setting of M0 and M1,
Are there any restrictions when switching settings during operation?
For example, Non-Circular 1/2→1/2 step→Non-Circular 1/2
Regards,
  • Hi user5287685,

    There are no restrictions. The change is immediate.

    Please note the following from the datasheet:

    Note that if the step mode is changed from full, ½, ¼, 1/8, or 1/16 to full, ½, ¼, 1/8, or 1/16 while stepping, the indexer will advance to the next valid state for the new MODE setting at the rising edge of STEP. If the step mode is changed from or to non-circular ½ step the indexer will go immediately to the valid state for that mode