According the Product Discontinuance Notification 20180715000.3 TI announced discontinuance of TO-263 and TO-220 packages affecting the part DRV102F/500, in the PDN TI recommend PN DRV104PWP as replacement with same functionality but not pin-for-pin equivalent and not exactly parametrically equivalent, according each datasheet the part should work as replacement except for the current rating, the driver DRV102F/500 support high output at 2.7A but the proposed DRV104PWP replacement driver only support 1.2A, there is one variant of this driver that remains as high-side switching and support 2.7A too?