This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8847EVM: SBW Connector

Part Number: DRV8847EVM
Other Parts Discussed in Thread: MSP-FET

I've purchased some of the DRV8847EVM Modules and plan to use these PCBs in a production environment.  I need to make some minor adjustments to the code as was wondering if a SBW connector is shipped with these evaluation boards?  My debugger is the MSP-FET.

If they do not come with an adapter, could you provide me with the PN for the 14pin to 4 pin adapter or provide me with the PNs of the connectors I will need to make this adapter?

Thanks for your help,

Joe