This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BOOSTXL-DRV8323RS: EVM cannot commutate motor in Six Pulse IPD mode; Rotor Align mode spins up and faults due to stall.

Part Number: BOOSTXL-DRV8323RS
Other Parts Discussed in Thread: MSP-EXP430F5529LP

New to BLDC motors, and having consistent issues. 

I am using a BOOSTSL-DRV8323RS as a gate driver and a MSP-EXP430F5529LP as a Launchpad to operate a A60-7XS V4 28-Pole kv330 motor.
I am running the BOOSTSL-DRV832x EVM. 

When attempting to operate in Six Pulse IPD Mode, the motor emits a single chirp and typically does not move. Any indication as to why this occurs would be great.

Additionally, when operating in Rotor Align Mode, the motor begins to commutate, increases in RPM and then faults consistently.
Is this part of the program or is there a way to resolve this issue?

I have tried to operate under many different configurations of parameters to no avail. 
The best results were under the following conditions attached in the

Sensorless Motor Control and Tuning
DRV832x Sensorless Software User's Guide
Device Configuration
Driver Utilized
DRV8323RS Sensorless
MODE

DRIVER ENABLE

Motor Control
MOTOR ENABLE

Set Motor Speed010020
20 %
Motor Direction
REVERSE
Motor Poles

PWM Switching Frequency
10
kHz

Motor Initial Position Mode

Status Report
FAULT STATUS INDICATOR
Electrical Speed
0 Hz
Current Motor Speed
0 RPM
 System Parameter Control
Min Off Duty
10
%

Min On Duty
15
%

Maximum Duty Cycle
100
%

Ramp Rate Delay
500
PWM Cycles

 Fault Handling Control
Under Voltage Limit
10
V

Over Voltage Limit
25
V

Stall Detect Rev Threshold
2
Revs

Stall Detect Timer Threshold
200
ms

Auto Fault Recovery Time
3000
ms

Motor Phase Current Limit
10
A

 Align Control
Align Sector
1
Align Wait Time
500
PWM Cycles

 Open Loop Acceleration Control
Acceleration Rate
4
Hz/s

Acceleration Stop
50000
mHz

Acceleration Velocity Constant
10000
mHz

 Closed Loop Control
BEMF Threshold
1000
counts

PWM Blank Counts
5
Clock Cycles

Startup Duty Cycle
4
%

Commutation Blank Time
5
PWM Cycles

Here is some specs on the motor.

Motor Technical Data: 
Powerrange:  max. 2300W (15 sec.) 
Idle Current at 8,4V: 1,5A  
inner resistance: 20mOhm  
RPM / Volt: 320  
Weight: 480g  
Diameter: 60 mm  
Length: 52 mm  
Type: 28-Pole  
recommended Timing: 25°  
Switching Frequency: 8 kHz 

Thank you.