Other Parts Discussed in Thread: LM317
Hello,
the datasheet (SLVSAB7D, p. 11) gives a pulldown resistance of "approximately 100 kΩ" for the I[4..0] inputs.
I've connected 2 of these inputs in parallel, pulling them via 1 kΩ to my supply of 5.1 V.
Can you imagine my surprise when measuring the voltage on the DRV8840 side of the resistor: 4.3 V ???
A bit of calculation gives a pulldown resistance of about 10 kΩ, which is by no way "approximately 100 kΩ" !
Am I correct that the datasheet needs some "rework" ?
Regards
...