Hi Team,
In the datasheet of DRV8872 the over-current condition, nFAULT pin of the IC (pin #4) will go low and the driver will try to recover in t_retry time. Customer tested this and found that the fault pin is not going low however the retry is happening attached is screenshot of the over-current test.
Dark Blue: Fault pin voltage
Light Blue: Output Current (5 A as measured in overcurrent condition)
Green: Output Voltage of one of the output pins
Can you please let me know why the pin is not going in fault.
Regards, Shinu Mathew.