This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BOOSTXL-DRV8323RS: What is the highest power BLDC motor ran with this EVM?

Part Number: BOOSTXL-DRV8323RS
Other Parts Discussed in Thread: MSP-EXP430F5529LP

What are the highest power motor(s) that are recommended or have been proven to work with the BOOSTXL-DRV8323RS and MSP-EXP430F5529LP?

  • Kenneth,

    The EVM is limited to 15A because of the traces and connectors. I don't have an example of high power but these are the design limitations. 

    Obviously the power on your end design can be much higher than this. The FET current rating as well as factors above are the limiting factor, not the DRV itself.

    Regards,

    -Adam