Other Parts Discussed in Thread: DRV8305
Hi Adam,
We are currently using the DRV8305NEPHPRQ1 in BLDC automotive application. We need a response ASAP. Please respond in a timely manner.
It appears Pins 29-32 are damaged internally on the chip. FETs for both the High side and Low side of the MOSFET Bridge circuit that connect to the pins seemed to be OK when isolated tests are performed for this phase of the motor.
Are there are any electrical measurement checks we can do, from our end, on these pins to verify the pins are functioning properly as we measure low resistance for that phase of the leg of the 3 phase motor. We would like to send over the DRV8305 to TI to analyze. If there is anyone at TI we can reach out directly to that would be great.
These tests were performed when running a high temp soak test (at 150C) with the load changing in a step wise pattern for the Motor. Our unit is failing now and everything is pointing towards these pins even after the unit is power cycled at room temperature. We are looking at all the possibilities where the DRV8305 maybe malfunctioning or the pins 29-32 are failing. The DRV8305 is being used in all our current units.
We are speculating that the charge pump on the DRV8305 may have been damaged in the process as well. The datasheet specifies the caps as 0.047micro Farad. Could you specify what the tolerance range for the charge pumps caps are?
Kindly provide any supporting information or what this error seems to suggest.
Best regards
Mohammad