The DRV8350RHRGZT driver chip has four pins (29, 30, 31, 32) to the bottom of the how to connect???
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The DRV8350RHRGZT driver chip has four pins (29, 30, 31, 32) to the bottom of the how to connect???
Hello,
Please check the datasheet, these pins are the hardware control pins. You will need to select the correct MODE, IDRIVE, and VDS for your application. If you need help, you can copy the EVM, the design files are available here: http://www.ti.com/lit/zip/slvc763
The EVM can be viewed and ordered here: http://www.ti.com/tool/DRV8350H-EVM
Pin 32 is no-connect.
Regards,
-Adam
Hello,
The EVM is for evaluation only and not to be used as a final product. The reason the EVM is limited is because the PCB is not designed for very high current operation. Please design your own board if you need more current.
Regards,
-Adam