Other Parts Discussed in Thread: BOOSTXL-DRV8323RS
Hi,
I'm trying to digest DRV8323RH's key features for the motor driver development of our company. I have a very basic question on 7 level input pin structure for idrive and VDS.
According to the datasheet there is a figure of seven level input structure (attached below). For me, it is not super clear. I have several questions to make it clear.
1) I tried to tie a node between R1 and R5 to DVDD or AGND. I checked Gate drive signal changed once I made a change. Are these configurations represent V_I7 (Maximum) and V_I1 (Minimum) state?
2) I don't get it what's the main difference between "75kohm to DVDD" and "75kohm to AGND", and how it should be configured. The default hardware setup is two 75kohm resistors are connected in series (R1 and R5). What's the state for this configuration? V_I5 or V_I3?
3) I'm wondering if only resistor value change in R1 and R2 make all 7 level configurations. If I want to change the state, do I need to replace 75kohms on R1 and R5 to others? Do I need to connect extra resistor on the middle node?
Since I'm the new user with this evaluation board, I need your help. I'm look forward to hearing from you soon. Thank you.