Other Parts Discussed in Thread: , CSD18531Q5A, DRV8886
Hi team,
My customer considers to use DRV8711 and he provided a question in terms of OCP threshold.
According to "DRV8711 Quick Spin and Tuning Guide", target over current protection level can be calculated by I_OCP = OCPTH / R_DS(ON) and Table 1(DRV8711EVM configuration) shows that I_OCP is set to 2A.
However, Ron of CSD18531Q5A is at most 5.8mΩ and even if we set OCPTH=250mV , I_OCP can be derived as 250mV/5.8mΩ=43A.
How can we derive 2A from I_OCP = OCPTH / R_DS(ON)?
Also, is OCP nothing to do with R_SENSE value?
I'm looking forward to hearing back from you.
Best regards,
Shota Mago