This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8703-Q1: PWM control mode

Part Number: DRV8703-Q1

hi

How to achieve the following PWM control mode? Mode=Hi-Z?

  • Hi Chen,

    There are two ways to achieve PWM control mode.

    1) Leave the MODE pin floating. There is an internal pullup and pulldown that will set the internal voltage at ~1.05V to enter PWM mode

    2) If using a GPIO on a mcu, set the GPIO as an input with no pullup or pulldown enabled.