This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV120: OK to power VIN after other inputs?

Part Number: DRV120

  My question is about power sequencing on the DRV120.  I'm powering the VIN input on my DRV120 from 24V.  The EN input goes to a 3.3V logic level GPIO on a microcontroller.  I have the STATUS port connected to an LED & resistor pulled up to 5V (lights when solenoid driven by OUT).  Due to the nature of our system, the 3.3V & 5V supplies come up 1st then the 24V supply comes up ~1 minute later.  Is there any issue w/ powering the DRV120 in this fashion?  Thx for any info.