This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8870: Does DRV8870 have a parameter for the back electromotive force?

Part Number: DRV8870

Dear all:

      We consider using DRV8870 for smart toilet motor control, Does DRV8870 have a parameter for the back electromotive force?

  If someone forcibly turns the motor from positive to negative, can the IC be protected?

  • User3830479,

    DRV8870 cannot report the back EMF. If someone forcibly turns the motor from positive to negative, a snubber or a voltage clamp circuit should be added to the input to protect the IC.

  • Dear wang Li:

        Thanks!  Can you help provide a snubber or a voltage clamp circuit for us?   It is for output or input?  I think it add in output PIN?

  • The back EFM can charge input capacitor voltage up through the switching FET's body. So, the system only needs one clamp circuit at input. If you put it at output, you may need two clamp circuit.

    Please search "tvs diode" and select a correct clamp voltage and current rating. And then, put it on your input.

  • The back EMF can charge the input capacitor voltage up through the switching FET's body. So, the system only needs one clamp circuit at input. If you put it at output, you may need two clamp circuits.

    Please search "tvs diode" and select a correct clamp voltage and current rating diode. And then, put it on your input.