Other Parts Discussed in Thread: DRV8842, , DRV8412, DRV8701EVM, DRV8701
Dear sir / madam,
We have used the TI H-bridge driver DRV8842 to successfully drive TECs that draw up to 4 A.
I am currently looking into driving larger TECs that initially draw 10A, 8V and then settle down to 6A, 8V.
I need t :
1) Reverse the polarity of the TECs depending on the context (hence the need for a full H-bridge).
2) Control the driver by PWM. I plan to start with a Beaglebone / Arduino board.
I believe that DRV8873 H-bridge motor driver fits the bill. Please let me know if there is a different chip you would recommend.
Thanks and regards,
~Ami