We are using 2 of this chip in our CAN module and we would like to put the module on sleep with the least possible standby current. Our target is <1mA, we pulled the nENBL pin to high to disable the outputs but we are still seeing 3.75mA. I looked at the DRV8803 datasheet and it only mentioned Supply current of 1.6mA typical and no mention about quiescent current during nENBL pulled high.
What is the Quiescent current of DRV8803 if nENBL pin is pulled to high (outputs disabled)?