This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2604L: probem, driver don't work after

Part Number: DRV2604L

Hello everyone,

I use a DRV2604L haptic driver an ERM "precision microdrive 304-103".

The configuration parameters are as follows:
at. ERM_LRA - ERM
b. FB_BRAKE_FACTOR [2: 0] - 2
c. LOOP_GAIN [1: 0] - 2
d. RATED_VOLTAGE [7: 0] - 2.7v (I use the formula in section 7.5.2.1)
e. OD_CLAMP [7: 0] - I use the formula in section 7.5.2.2 for V (ERM_clamp) = 2.7v for security
f. AUTO_CAL_TIME [1: 0] - 3
g. DRIVE_TIME [3: 0] - hexadecimal value: 0x1B
h. SAMPLE_TIME [1: 0] - 3
i. BLANKING_TIME [3: 0] - 1
j. IDISS_TIME [3: 0] - 1
k. ZC_DET_TIME [1: 0] - 0

VDD is between 3.2 and 4.2v (lithium element)
The integration scheme has been respected.

For each ERM, I do the autocalibration procedure.

However, after several waveform cycles (around 50 to 200) of each ERM (open or closed loop mode), the driver fails.

A reset or a power-up does not allow to re-pilot it and to make a waveform cycles or a procedure of autocalibration. 

It was like this that the driver was definitely broken.  But the ERM are good...

I have this problem on several copies of my product.

An idea ?