For OUT1 & OUT2 terminals, per datasheet it says "Connect directly to the motor, or other inductive load". For EMC related issues, if inductors are put in series from the two output terminals to the pump terminals, what would the impact to pump driving performance considering the pump is a inductive load anyway?