I am using the Vref 5 Volt output (pin 2) to set a current limit reference voltage. Can the Vref pin have a 47uF tantalum capacitor connected to ground and be safe for the IC chip when the input VDD supply is shut down? Is there protection inside the chip to be able to discharge the capacitor rapidly during power-down? I need an answer as soon as possible.