The software path I used: DRV830x-HC-C2-KIT_v105\GUI_project_InstaSPIN_BLDC
Maxon parameters are as follows:
Nominal voltage V 24
No load speed rpm 60800
No load current mA 282
Nominal speed rpm 57500
Nominal torque (max. continuous torque) mNm 23.6
Nominal current (max. continuous current) A 6.45
Stall torque mNm 561
Stall current A 149
Max. efciency % 91.6
Terminal resistance Ohm 0.161
Terminal inductance mH 0.0171
Torque constant mNm/A 3.76
Speed constant rpm/V 2540
Speed/torque gradient rpm/mNm 109
Mechanical time constant ms 2.04
Rotor inertia gcm 1.79
1. When EnableFlag=1,Set the motor speed at 500rpm, the motor runs normally, When the motor is loaded, the motor runs abnormally or even stops running.
How to solve the problem of on-load operation of the motor?
2. I used Instaspin foc to drive the motor mentioned above. The motor run normally 500rpm, When the motor is loaded, the motor can still operate normally.
How to solve the problem of Instaspin BLDC on-load operation?